3.1.2 TCM Performance on PIC32CZ CA90 Curiosity Ultra Evaluation Board

Download

Description

The application demonstrate code execution from various memory locations and compares the time taken to execute the code from Flash memory, SRAM, and TCM with and without the Instruction Cache and Data Cache. The result is displayed MPLAB Data Visualizer Serial Console.

Modules/Technology Used

  • Peripheral Modules
    • PORT
    • EVSYS
    • SERCOM - UART
  • System Services
    • STDIO

Hardware Used

Software/Tools Used

This project has been verified to work with the following versions of software tools:

Refer to the Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/pic32cz_ca90_cult.

  • Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version
  • Any Serial Terminal application, such as Tera Term terminal application

Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).

Setup

  • Connect the Type-A male to Micro-B USB cable to the Micro-B DEBUG USB port to power and debug the PIC32CZ CA90 Curiosity Ultra evaluation board. Connect the External Power Supply (6.5V to 14V) to the J100 connector

Programming Hex File

The pre-built hex file can be programmed by following the below steps.

Steps to program the hex file
  • Open MPLAB X IDE
  • Close all existing projects in IDE, if any project is opened
  • Go to File>Import>Hex/ELF file
  • In the Import Image File window,
    1. Create Prebuilt Project,
      • Click the Browse button to select the prebuilt hex file
      • Select Device as PIC32CZ8110CA90208
      • Ensure the proper tool is selected under Hardware Tool and click the Next button
    2. Select Project Name and Folder,
      • Select appropriate project name and folder and click the Finish button
  • In MPLAB X IDE, click the Make and Program Device button to program the device
  • Follow the steps in Running the Demo section below

Programming/Debugging Application Project

  • Open the project (pic32cz_ca90_tcm_performance\firmware\tcm_performance_pic32cz_ca90_cult.X) in MPLAB X IDE
  • Ensure PIC32CZ CA90 Curiosity Ultra is selected as hardware tool to program/debug the application
  • Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
  • Follow the steps in Running the Demo section below

Running the Demo

  • After building the application and completing the programming, open the MPLAB Data Visualizer by clicking the highlighted icon below
  • Configure the serial port setup of the PIC32CZ CA90 Curiosity Ultra evaluation board by clicking the Gear icon shown below
  • Set the 115200 as baudrate in the COM setting
  • Open the Serial Port of the PIC32CZ CA90 Curiosity Ultra evaluation board by clicking the Play icon as follows
  • Select the Send to Terminal to visualize the TCM Performance Test Results and click Close
  • Press the RESET push button on the evaluation board to reset the device
  • Observe the console message TCM Performance Comparison on the MPLAB Data Visualizer

Comments