3.1.4 Getting Started Application Using Harmony v3 Drivers on PIC32CZ CA90 Curiosity Ultra Development Board
Description
The application reads the current room temperature from the temperature sensor on the I/O1 Xplained Pro Extension kit. The temperature reading is displayed on a serial console periodically every second. In addition, the application writes the temperature readings to EEPROM. When a character is entered on the console, the last five written temperature values are read from the EEPROM and displayed on the console. An LED (LED0) on the PIC32CZ CA90 Curiosity Ultra board is toggled every time the temperature is displayed on the serial console.
Modules/Technology Used
- Peripheral Modules
- PORT
- Clock
- EVSYS
- USART
- TCC0
- DMA
- SERCOM
- NVIC
- Drivers
- USART
- I2C
- System Services
- Time
The following figure provides the MCC Harmony project graph with all the components.

Hardware Used
Software/Tools Used
Refer to the Project Manifest present in harmony-manifest-success.yml under
the project folder
pic32cz_ca90_cult_getting_started_drv/firmware/src/config/pic32cz_ca90_cult.
- Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version
Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Verify that the I/O1 Xplained Pro Extension kit (temperature sensor) is connected to Extension Header 1 (EXT1) on the PIC32CZ CA90 Curiosity Ultra development board
- Connect the Type-A male to Micro-B
USB cable to Micro-B DEBUG USB port (J200) to program and debug the PIC32CZ CA90
Curiosity Ultra development board and connect to a external power supply (6.5V to 14V)
to power-up the board
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
Steps to program the hex file- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened
- Go to File>Import>Hex/ELF file
- In the Import Image File window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file
- Select Device as PIC32CZ8110CA90208
- Ensure the proper tool is selected under Hardware Tool and click the Next button
- Select Project Name and Folder,
- Select appropriate project name and folder and click the Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click the Make and Program Device button to program the device
- Follow the steps in Running the Demo section below
Programming/Debugging Application Project
- Open the project
(
pic32cz_ca90_cult_getting_started_drv/firmware/pic32cz_ca90_cult.X)in MPLAB X IDE - Ensure
PIC32CZ CA90 Curiosity Ultrais selected as hardware tool to program/debug the application - Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo
- Open the Tera Term terminal application on the PC (from the Windows Start menu by pressing the Start button)
- Change the baud rate to 115200
- The user should see the temperature
values (in °F) being displayed on the terminal every 500 milliseconds, as shown
below

- Notice the LED0 blinking at 1 second rate
- Press any character on the terminal
to display the last five values written to the EEPROM
- The user may vary the temperature by
placing the finger on the temperature sensor (for a few seconds)
Comments
- Reference Training Module: Getting Started with MPLAB® Harmony v3 Drivers and System Services on SAM E70/S70/V70/V71 MCUs.
- This application demo builds and
works out of box by following the instructions above in Running the Demo section. If
the user needs to enhance/customize this application demo, should use the MPLAB
Harmony v3 Software framework. Refer to the following links to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232)
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253)
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project