5.2.2 .fillvalue [value]
Define the byte value to be used as fill in a code section when the lower
word (bits 0-15) is skipped due to alignment or data defining directives. If value is not
specified, the default value of 0x0000 is used. Directives that may cause the lower word to
filled are: .align, .fill, .skip,
.org and .space. The value is persistent for a given
code section, throughout the entire source file, and may be changed to another value by
issuing subsequent .fillvalue directives.
See the Section Example table.