12.7 Creating an Incrementing Modulo Buffer in X Memory
An incrementing modulo buffer for use in assembly language can be easily
         defined in C. In this example, the macro _XBSS is used to define an array
         whose memory alignment is the smallest power of two that is greater than or equal to its
         size. _XBSS is defined in the device header file, which in this example is
            p30F6014.h. The generic header file xc.h is used
         to access this device header file.
#include "xc.h"
#include "stdio.h"
int _XBSS(128) xbuf[50];
void main()
{
  printf("Should be zero: %x\n", (int) &xbuf % 128);
}
      The equivalent definition in assembly language appears below. The section alignment could have specified with a separate .align directive. By using * as a section name, the linker is afforded maximum flexibility to allocate memory.
       .global _xbuf
       .section *,xmemory,bss,align(128)
_xbuf: .space 100