12.2 Locating a Variable at a Specific Address
In this example, array buf1 is located at a specific
         address in data memory. The address of buf1 can be confirmed by executing
         the program in the simulator, or by examining the link map.
#include "stdio.h"
int __attribute__((address(0x900))) buf1[128];
void main()
{
  printf("0x900 = 0x%x\n", &buf1);
}
      The equivalent array definition in assembly language appears below. The
            .align directive is optional and represents the default alignment in
         data memory. Use of * as a section name causes the assembler to generate a
         unique name based on the source file name.
       .section *,address(0x900),bss,near
       .global _buf1
       .align 2
_buf1: .space 256