8.2 Linker Usage
The MPLAB XC-DSC Object Linker translates object files from the MPLAB XC-DSC assembler, and archive/library files from the MPLAB XC-DSC archiver/librarian, into an executable file. See the MPLAB® XC-DSC C Compiler User’s Guide (DS-50003589) for an overview of the tools process flow.
In most instances it will not be necessary to invoke the linker directly,
         as the compiler driver, xc-dsc-gcc, will
         automatically execute the linker with all necessary arguments. Using the linker directly is
         not simple, and should be attempted only by those with a sound knowledge of the compiler
         and linking in general. The compiler often makes assumptions about the way in which the
         program will be linked. If the linker sections are not linked correctly, code failure may
         result.