3.5.3 -p,
--processor=PROC
Specify the target processor, e.g.:
xc-dsc-as -p33EP32MC504 file.s
The assembler defines macros based on the target processor setting, which
can be tested by conditional directives in source code. For example, include file
p33EP32MC504.inc contains the following:
.ifndef __33EP32MC504
.error “Include file does not match processor setting”
.endif
In addition to the target processor, a macro to identify the device family is also defined. For example:
.ifdef __dsPIC33E
.print “dsPIC33E family selected”
.endif
Macros for the device families (see Predefined Symbols) are defined based on target processor setting.