2.5.3.2 Program boot.bin to the NAND Flash Memory
To program the boot.bin file on the SAM9X60-Curiosity board, use the following command:
sam-ba -p serial -b sam9x60-curiosity -a nandFlash -c writeboot:boot.bin -c verifyboot:boot.bin //write and verify bootstrap image
Note: Ensure that the directory from which the command is run contains
the generated boot.bin file.