4 Appendix B: Configure at91bootstrap for Debug Use with MPLAB X IDE
All preconfigured applications are available in at91bootstrap→ configs. The build called sam9x60_curiosity_bkptnone_defconfig can only be used to debug the application using MPLAB X IDE. See the following note.
Note: <board_name>_bkptnone_defconfig configures
at91bootstrap to continuously loop at the end of its execution so that the debugger can
take control (a time-out message is displayed) and continue to download the application
into user space. Therefore, bkptnone_defconfig should be used only to debug the
bootstrap using MPLAB X IDE.
Go to Project→ Properties→ Kconfig→ Load→ Harmony3→ at91bootstrap→ configs→ sam9x60_curiosity_bkptnone_defconfig→ Open.
This provides the Kconfig file configuration required to build at91bootstrap for debug use with MPLAB X IDE.
Build this at91bootstrap configuration as described in Prepare the Programming Environment.