2.5 Get Device Support for MPLAB X IDE
Use the MPLAB Pack Manager, found under Tools→Packs, to add support for new devices in MPLAB X.
For the PIC18 family, update to the latest version by performing the following steps:
- Click Check for Updates.
- For the PIC18 family, select the latest available version of PIC18F-J_DFP, PIC18F-K_DFP, PIC18F-Q_DFP or PIC18Fxxxx_DFP Device Support. If necessary, do the same for PIC16 Device Support (PIC16..._DFP).
- Click Install.
For offline installers, go to packs.download.microchip.com. Double click the installer file and follow the instructions to install a package. Any open MPLAB X window must be closed for the installation to take effect.
- Plug-ins can also be installed in
MPLAB X IDE. Go to the file menu, then Tools>Plugins Download.
Figure 2-6. Plugins Download
- Go to MPLAB X Plugin Manager to see
the available plug-ins.
Figure 2-7. Available Plug-ins