3.4.4 Functional Description
The NAND Flash sector size is programmable and can be set to 512 bytes or 1024 bytes. The PMECC module generates redundancy at encoding time, when a NAND write page operation is performed. The redundancy is appended to the page and written in the spare area. This operation is performed by the processor. It moves the content of the PMECCx registers into the NAND Flash memory. The number of registers depends on the selected error correction capability (see Table 3-12). This operation is executed for each sector. At decoding time, the PMECC module generates the remainder of the received codeword by minimal polynomials. When all polynomial remainders for a given sector are set to zero, no error occurred. When the polynomial remainders are other than zero, the codeword is corrupted and further processing is required.
The PMECC generates an interrupt indicating that an error occurred. The processor must read the Interrupt Status register (PMECC_ISR). This register indicates which sector is corrupted.
To find the error location within a sector, the processor must execute the following decoding steps:
- Syndrome computation
- Find the error locator polynomials
- Find the roots of the error locator polynomial
All decoding steps involve finite field computation, for which a library of finite field arithmetic must be available to perform addition, multiplication and inversion. The finite field arithmetic operations can be performed through the use of a memory mapped lookup table, or direct software implementation. The software implementation presented is based on lookup tables. Two tables named gf_log and gf_antilog are used. If alpha is the primitive element of the field, then a power of alpha is in the field. Assume beta = alpha ^ index, then beta belongs to the field, and gf_log(beta) = gf_log(alpha ^ index) = index. The gf_antilog tables provide exponent inverse of the element, if beta = alpha ^ index, then gf_antilog(index) = beta.
The first step consists of the syndrome computation. The PMECC computes the remainders and software must substitute the power of the primitive element.
The procedure implementation is described in Remainder Substitution Procedure.
The second step is the most software intensive. It is the Berlekamp’s iterative algorithm for finding the error-location polynomial.
The procedure implementation is described in Find the Error Location Polynomial Sigma(x).
The last step is finding the root of the error location polynomial. This step can be very software intensive, as there is no straightforward method of finding the roots, except by evaluating each element of the field in the error location polynomial. However, a hardware accelerator can be used to find the roots of the polynomial. The Programmable Multibit Error Correction Code Location (PMERRLOC) module provides this type of hardware acceleration.