32.2.2 Push-Pull Mode
In Push-Pull mode, two output signals are generated, alternating copies of the input as illustrated in Figure 32-3. This alternation creates the Push-Pull effect required for driving some transformer-based power supply designs. Steering modes are not used in Push-Pull mode. A basic block diagram for the Push-Pull mode is shown in Figure 32-4.
The Push-Pull sequencer is reset whenever EN = 0 or if an
auto-shutdown event occurs. The sequencer is clocked by the first input pulse, and the
first output appears on CWGxA.
The unused outputs CWGxC and CWGxD drive copies of CWGxA and CWGxB, respectively, but with polarity controlled by the POLC and POLD bits, respectively.
‘b101)