6.1.9.15 End Directive

The END label directive is optional, but if present should be at the very end of the program. It will terminate the assembly and not even blank lines should follow this directive.

If an expression is supplied as an argument, that expression will be used to define the entry point of the program. This is stored in a start record in the object file produced by the assembler. Whether this is of any use will depend on the linker.

For example:

END  start_label  ;defines the entry point

or

END               ;do not define entry point