6.1.9.10 DDW Directive
The DDW
directive is used to initialize 32-bit words of
program memory.
The directive takes a comma-separated list of arguments. Each argument can be a numeric
value (e.g., 55
), a character constant (e.g. 'T'
), or a
string (e.g. "level"
or 'level'
). Each argument or each
character of a string argument is written as four bytes into consecutive program memory
locations within the current psect.
In the following code:
PSECT myWords,class=CODE,delta=2
alabel:
DDW 'X',1,2,398,0x8005FFFF
the DDW
directive will initialize each word of program
memory with the supplied value, specifically (in hexadecimal):
00000058 00000001 00000002 0000018E 8005FFFF
DDW
directive, for
example:PSECT myConst,class=CODE,delta=1
words:
DDW "a terminated string",0
will
define:00000061 00000020 00000074 00000065 00000072 0000006D 00000069 0000006E 00000061 00000074
00000065 00000064 00000020 00000073 00000074 00000072 00000069 0000006E 00000067 00000000
The DDW
directive cannot be used to created objects in data memory. For
that, use the DS
directive (see 6.1.9.13 Ds Directive).