4.6.1 Options Specific to PIC Devices
The options shown in the table below are useful when compiling for 8-bit Microchip PIC devices with the MPLAB XC8 compiler and are discussed in the sections that follow.
Option (links to explanatory section) | Controls |
---|---|
-maddrqual=action | How the compiler will respond to storage qualifiers. |
-mchecksum=specs | The generation and placement of a checksum or hash. |
-mcodeoffset=offset | The offset applied to reset and interrupt vectors. |
-m[no-]config | Whether the device will be programmed with default configuration bit values. |
-mcpu=device | The target device that code will be built for. |
-mdebugger=type | Which debugger will be in use when executing the code. |
-m[no-]default-config-bits | See -m[no-]config . |
-mdfp=path | Which device family pack to use. |
-m[no-]download | How the final HEX file is conditioned. |
-m[no-]download-hex | See -m[no-]download . |
-memi=mode | The external memory interface that will be used. |
-merrata=type | Which workarounds to errata will be applied by the compiler. |
-mheap=size | The maximum allowable size for the heap. |
-m[no-]ivt=address | The interrupt vector table selected at startup. |
-m[no-]keep-startup | Whether the runtime startup source is deleted after compilation. |
-mmaxichip | Use of a hypothetical device with full memory. |
-m[no-]osccal | Whether the oscillator will be calibrated. |
-m[no-]oscval=value | The oscillator calibration value. |
-mram=ranges | Data memory that is available for the program. |
-mreserve=space@start:end | The address ranges in the memory space to be reserved. |
-m[no-]resetbits | Whether the device status bits should be preserved. |
-mrom=ranges | Program memory that is available for the program. |
-m[no-]save-resetbits | See -m[no-]resetbits . |
-mshroud | Whether the output file should obfuscate the source code. |
-msmart-io-format="fmt" | The functionality (size) of formatted IO functions linked in. |
-mstack=model[:size] | Which data stack will be used by default. |
-m[no-]stackcall | Whether functions can be called via lookup tables. |
-msummary=types | What memory summary information is produced. |
-mundefints=action | How the compiler completes unimplemented interrupts. |
-m[no-]use-ivt | see -m[no-]ivt . |