3.4.11 How Can I Implement a Delay in My Code?
If an accurate delay is required, or if there are other tasks that can be performed during the delay period, then using a timer to generate an interrupt is the best way to proceed.
If these are not issues in your code, then you can use the compiler’s
in-built delay pseudo-functions: _delay(),
__delay_ms() or __delay_us() (see _delay Builtin). These all expand
into in-line assembly instructions or a (nested) loop of instructions that will consume
the specified number of cycles or time. The delay argument must be a constant expression
(i.e. it cannot contain variables or function calls) and evaluate to less than
50,463,240. To use the __delay_ms() or __delay_us()
versions of the delay, the preprocessor macro _XTAL_FREQ must be
correctly defined to match the device clock frequency.
Note that these code sequences will only use the nop
instruction and/or instructions which form a loop. The alternate watchdog versions of
these pseudo-functions, e.g., _delaywdt(), can use the
clrwdt instruction as well.