3.2.6 How Do I Build Libraries?
When you have functions and data that are commonly used in applications, you can make all the C source and header files available so other developers can copy these into their projects. Alternatively, you can build these modules into object files and package them into library archives, which, along with the accompanying header files, can then be built into an application.
Libraries can be more convenient because there are fewer files to manage. However, libraries do need to be maintained. MPLAB XC32 uses *.a library archives. Be sure to rebuild your library objects when you move your project to a new release of the compiler toolchain.
Using the compiler driver, libraries can begin to be built by listing all
the files that are to be included into the library on the command line. None of these files
should contain a main() function, nor settings for configuration bits or
any other such data.
For information on how to create your own libraries, see 5.4.1 Library Files, "User-Defined Libraries" sub-section.