5.7.1.14 Malloc-variant Option
The -mmalloc-variant=scheme option indicates to the compiler
the scheme of dynamic memory allocation that should be employed for the program. See
Dynamic Memory Allocation for more
information on this type of memory allocation and the heap, from which allocation takes
place.
The -mmalloc-variant=lite form of this option selects a simple scheme
that will yield the smallest code size. It might, however, result in a fragmented heap
when freeing allocated memory, preventing further memory from being allocated at
runtime. This is the default scheme if no option is specified.
The -mmalloc-variant=binned option uses a more sophisticated allocation scheme
that will result in less fragmentation, but at the expense of increased code size.