27.3 __builtin_bswap32 Built-in Function
Returns its argument with the order of its bytes reversed. For example, an argument value of 0xaabbccdd is returned as 0xddccbbaa. A byte here always means exactly 8 bits.
Prototype
uint32_t __builtin_bswap32 (uint32_t x)
Argument
x: the value whose bytes are to be swapped
Return Value
The byte-swapped value
Error Messages
None.