27.5 __builtin_has_attribute Built-in Function
The __builtin_has_attribute built-in function evaluates to an integer
constant expression. This expression is true if the symbol or type referenced by the
built-in function's first argument has been declared with the attribute referenced by
its second argument; false otherwise. Neither argument is evaluated. The first argument
is subject to the same restrictions as the argument to typeof, and when
it does not reference a symbol, the type of this expression is considered. This built-in
function cannot be used as the argument to #if or
#elif preprocessor directives.
The attribute argument is an attribute name optionally followed by a comma-separated list of attribute arguments enclosed in parentheses. Both forms of attribute names—with and without double leading and trailing underscores—are recognized. If no arguments are specified with an attribute that expects one or more arguments, the built-in function considers only if its first argument has been declared with the attribute and ignores any attribute argument. When an incomplete set of attribute arguments have been specified, the built-in function returns true if all specified arguments match.
x is declared with the aligned attribute, but the
second usage evaluates to false because x is declared aligned
(8) and not aligned
(4).attribute ((aligned (8))) int x;
_Static_assert (__builtin_has_attribute (x, aligned), "aligned");
_Static_assert (!__builtin_has_attribute (x, aligned (4)), "aligned (4)"); Due to a limitation, the __builtin_has_attribute built-in function
always returns false when checking for the mode attribute, even if that
attribute was used with the declaration of the type or variable referenced by the first
argument. The function does not support checking of labels or C enumerators as the first
argument.
Prototype
bool __builtin_has_attribute (type-or-expression, attribute)
Argument
type-or-expression: the symbol to check
attribute: the attribute to check against
Return Value
A true or false value
Error Messages
None.