27.7 ACLE Built-in Functions
A subset of the features defined by the Arm C Language Extensions are provided by
<arm_acle.h> as built-in functions by MPLAB XC32. These
functions are tabulated below, and further information on their operation can be
obtained from 2024 Arm C Language specification.
| Function prototype | Description |
|---|---|
uint32_t __sadd8(uint32_t op1, uint32_t op2) |
Performs four parallel signed 8-bit additions. |
uint32_t __qadd8(uint32_t op1, uint32_t op2) |
Performs four parallel signed 8-bit additions with saturation. |
uint32_t __shadd8(uint32_t op1, uint32_t
op2) |
Performs four parallel signed 8-bit additions, then divides each sum by 2. |
uint32_t __uadd8(uint32_t op1, uint32_t op2) |
Performs four parallel unsigned 8-bit additions. |
uint32_t __uqadd8(uint32_t op1, uint32_t
op2) |
Performs four parallel unsigned 8-bit additions with saturation. |
uint32_t __uhadd8(uint32_t op1, uint32_t
op2) |
Performs four parallel unsigned 8-bit additions, then divides each sum by 2. |
uint32_t __ssub8(uint32_t op1, uint32_t op2) |
Performs four parallel signed 8-bit subtractions. |
uint32_t __qsub8(uint32_t op1, uint32_t op2) |
Performs four parallel signed 8-bit subtractions with saturation. |
uint32_t __shsub8(uint32_t op1, uint32_t
op2) |
Performs four parallel signed 8-bit subtractions, then divides each difference by 2. |
uint32_t __usub8(uint32_t op1, uint32_t op2) |
Performs four parallel unsigned 8-bit subtractions. |
uint32_t __uqsub8(uint32_t op1, uint32_t
op2) |
Performs four parallel unsigned 8-bit subtractions with saturation. |
uint32_t __uhsub8(uint32_t op1, uint32_t
op2) |
Performs four parallel unsigned 8-bit subtractions, then divides each difference by 2. |
uint32_t __sadd16(uint32_t op1, uint32_t
op2) |
Performs two parallel signed 16-bit additions. |
uint32_t __qadd16(uint32_t op1, uint32_t
op2) |
Performs two parallel signed 16-bit additions with saturation. |
uint32_t __shadd16(uint32_t op1, uint32_t
op2) |
Performs two parallel signed 16-bit additions, then divides each sum by 2. |
uint32_t __uadd16(uint32_t op1, uint32_t
op2) |
Performs two parallel unsigned 16-bit additions. |
uint32_t __uqadd16(uint32_t op1, uint32_t
op2) |
Performs two parallel unsigned 16-bit additions with saturation. |
uint32_t __uhadd16(uint32_t op1, uint32_t
op2) |
Performs two parallel unsigned 16-bit additions, then divides each sum by 2. |
uint32_t __ssub16(uint32_t op1, uint32_t
op2) |
Performs two parallel signed 16-bit subtractions. |
uint32_t __qsub16(uint32_t op1, uint32_t
op2) |
Performs two parallel signed 16-bit subtractions with saturation. |
uint32_t __shsub16(uint32_t op1, uint32_t
op2) |
Performs two parallel signed 16-bit subtractions, then divides each difference by 2. |
uint32_t __usub16(uint32_t op1, uint32_t
op2) |
Performs two parallel unsigned 16-bit subtractions. |
uint32_t __uqsub16(uint32_t op1, uint32_t
op2) |
Performs two parallel unsigned 16-bit subtractions with saturation. |
uint32_t __uhsub16(uint32_t op1, uint32_t
op2) |
Performs two parallel unsigned 16-bit subtractions, then divides each difference by 2. |
int32_t __ssat16(int32_t x, const unsigned int
sat_width) |
Saturates each 16-bit halfword of a 32-bit integer to a specified signed bit width. |
uint32_t __usat16(uint32_t x, const unsigned int
sat_width) |
Saturates an unsigned integer to the range of an unsigned 16-bit integer. |
uint32_t __smlad(uint32_t op1, uint32_t op2, uint32_t
op3) |
Performs two signed 16x16-bit multiplications and accumulates the results. |
uint32_t __smuad(uint32_t op1, uint32_t op2) |
Performs two signed 16x16-bit multiplications and returns the sum of the products. |
uint32_t __smlsd(uint32_t op1, uint32_t op2, uint32_t
acc) |
Performs two signed 16x16-bit multiplications and subtracts the result from an accumulator. |
uint64_t __smlald(uint32_t op1, uint32_t op2, uint64_t
acc) |
Performs two signed 16x16-bit multiplications and accumulates the results into a 64-bit accumulator. |
uint32_t __smlabb(uint32_t value1, uint32_t value2, uint32_t
value3) |
Performs a signed multiply-accumulate on the lower 16-bit halfword of
|
uint32_t __smlabt(uint32_t value1, uint32_t value2, uint32_t
value3) |
Performs a signed multiply-accumulate on the lower 16-bit halfword of
|
uint32_t __smlatb(uint32_t value1, uint32_t value2, uint32_t
value3) |
Performs a signed multiply-accumulate on the upper 16-bit halfword of
|
uint32_t __smlatt(uint32_t value1, uint32_t value2, uint32_t
value3) |
Performs a signed multiply-accumulate on the upper 16-bit halfword of
|
uint32_t __smlawb(uint32_t value1, uint32_t value2, uint32_t
value3) |
Performs a signed multiply-accumulate between a 32-bit operand and
the lower 16-bit halfword of another operand, then accumulates the
result with |
uint32_t __smlawt(uint32_t value1, uint32_t value2, uint32_t
value3) |
Similar to |
int32_t __smmls(int32_t value1, int32_t value2, int32_t
value3) |
Performs a signed multiply-subtract operation with the most significant word of the product. |
int32_t __smmlar(int32_t value1, int32_t value2, int32_t
value3) |
Performs a signed multiply-accumulate operation with rounding and the most significant word of the product. |
int32_t __smmlsr(int32_t value1, int32_t value2, int32_t
value3) |
Performs a signed multiply-subtract operation with rounding and the most significant word of the product. |
int32_t __smmulr(int32_t value1, int32_t
value2) |
Performs a signed multiply operation with rounding and returns the most significant word of the product. |
uint32_t __smulbb(uint32_t value1, uint32_t
value2) |
Executes a signed multiply between the lower 16-bit halfwords of both operands. |
uint32_t __smulbt(uint32_t value1, uint32_t
value2) |
Executes a signed multiply between the lower 16-bit halfword of
|
uint32_t __smultb(uint32_t value1, uint32_t
value2) |
Executes a signed multiply between the upper 16-bit halfword of
|
uint32_t __smultt(uint32_t value1, uint32_t
value2) |
Executes a signed multiply between the upper 16-bit halfwords of both operands. |
uint32_t __smulwb(uint32_t value1, uint32_t
value2) |
Executes a signed multiply between a 32-bit operand and the lower 16-bit halfword of another operand. |
uint32_t __smulwt(uint32_t value1, uint32_t
value2) |
Similar to __smulwb but operates on the upper 16-bit halfword of the second operand. |
uint64_t __umaal(uint32_t value1, uint32_t value2, uint32_t
value3, uint32_t value4) |
Performs an unsigned multiply-accumulate long operation. |
uint64_t __smlalbb(uint32_t value1, uint32_t value2, uint64_t
value3) |
Performs a signed multiply-accumulate long operation on the lower 16-bit halfwords of both operands. |
uint64_t __smlalbt(uint32_t value1, uint32_t value2, uint64_t
value3) |
Performs a signed multiply-accumulate long operation on the lower
16-bit halfword of |
uint64_t __smlaltb(uint32_t value1, uint32_t value2, uint64_t
value3) |
Performs a signed multiply-accumulate long operation on the upper
16-bit halfword of |
uint64_t __smlaltt(uint32_t value1, uint32_t value2, uint64_t
value3) |
Performs a signed multiply-accumulate long operation on the upper 16-bit halfwords of both operands. |