4.2 CLASSB_CPU_RegistersTest
Function
CLASSB_TEST_STATUS CLASSB_CPU_RegistersTest(bool running_context);
Summary
This self-test checks the processor core registers of the CPU, to detect stuck-at faults.
Description
This self-test writes test patterns into the processor core registers, and special function registers, and read them back to detect stuck-at faults. Special function register bits which are reserved or should not be modified during the test are not written.
When the 'Test FPU Registers?' option is selected, the FPU registers will be tested.
Precondition
None.
Parameters
running_context - False for startup test. True for run-time test.
Returns
CLASSB_TEST_STATUS - Status of the test.
Example
CLASSB_TEST_STATUS classb_test_status = CLASSB_TEST_NOT_EXECUTED;
// Perform run-time test of the CPU registers
classb_test_status = CLASSB_CPU_RegistersTest(true);
Remarks
This self-test can be used during startup as well as run-time. If a failure is detected, this self-test remains in an infinite loop to avoid unsafe code execution.