4.15 CLASSB_SST_WDT_Recovery
Function
static void CLASSB_SST_WDT_Recovery(void);
Summary
This function is called if a WDT reset is caused while a startup self-test is running.
Description
This function is used inside the CLASSB_Init() function. When the device comes back from a WDT reset, if there has been a startup self-test running, it is assumed that the WDT reset has happened because a Class B self-test has taken more time that the WDT timeout period. In this case, the CLASSB_SST_WDT_Recovery() function is called from CLASSB_Init().
Precondition
None.
Parameters
None.
Returns
None.
Example
if ((RSTC_REGS->RSTC_RCAUSE & RSTC_RCAUSE_WDT_Msk) == RSTC_RCAUSE_WDT_Msk)
{
if (*classb_test_in_progress == CLASSB_TEST_STARTED)
{
CLASSB_SST_WDT_Recovery();
}
}
Remarks
This function is for the internal use of the Class B library.