4.1 CLASSB_App_WDT_Recovery

Function

static void CLASSB_App_WDT_Recovery(void);

Summary

This function is called if a WDT reset is caused during run-time.

Description

This function is used inside the CLASSB_Init() function. When the device comes back from a WDT reset, if a WDT test by the Class B library has not been in progress, it is assumed that the WDT reset has happened since the application failed to clear the WDT during regular intervals. In this case, the CLASSB_App_WDT_Recovery() function is called from CLASSB_Init().

Precondition

None.

Parameters

None.

Returns

None.

Example

if ((RSTC_REGS->RSTC_RCAUSE & RSTC_RCAUSE_WDT_Msk) == RSTC_RCAUSE_WDT_Msk)
{
    if (!(*wdt_test_in_progress == CLASSB_TEST_STARTED))
    {
        CLASSB_SST_WDT_Recovery();
    }
}

Remarks

This function is for the internal use of the Class B library.