28.5.2.1 Initialization
Before enabling event routing within the system, the Event Users Multiplexer
and Event Channels must be selected in the Event System (EVSYS), and the two peripherals
that generate and use the event must be configured. Follow these steps to configure the
event:
- In the peripheral generating the event, enable output of event by writing a '1' to the respective Event Output Enable bit ("EO") in the peripheral's Event Control register, for example, AC.EVCTRL.WINEO0 or RTC.EVCTRL.OVFEO.
- Configure the EVSYS:
- Configure the Event User multiplexer by writing the respective EVSYS.USERm register, refer to 28.5.2.3 User Multiplexer Setup.
- Configure the Event Channel by writing the respective EVSYS.CHANNELn register, refer to 28.5.2.4 Event System Channel.
- Configure the action to be executed
by the event user peripheral by writing to the Event Action bits (EVACT) in the
respective Event control register, for example, TC.EVCTRL.EVACT, PDEC.EVCTRL.EVACT.
Note: This step is not applicable for all the peripherals.
- In the event user peripheral, enable event input by writing a '1' to the respective Event Input Enable bit ("EI") in the peripheral's Event Control register, for example, AC.EVCTRL.IVEI0, ADC.EVCTRL.STARTEI.