2.3 Configure LAN8651 Support on SAM E54 Xplained Pro Evaluation Kit Target
- Before continuing, make sure the
virtual environment is activated.
$ source ~/zephyrproject/.venv/bin/activate
- Enter the directory.
$ cd zephyrproject/zephyr/
-
Open the same54_xpro.dts file.
$ vim boards/atmel/sam0/same54_xpro/same54_xpro.dts
- In the file make the adaptations as
listed below (marked bold in the code section):
- Add &dmac node between &sercom2 node and &sercom4 node.
- Add the MAC and PHY node contents inside &sercom4 node.
- Disable &gmac and &mdio nodes statuses.
/* * Copyright (c) 2019 Benjamin Valentin # Copyright (c) 2024-2025 Gerson Fernando Budke <nandojve@gmail.com> * * SPDX-License-Identifier: Apache-2.0 */ /dts-v1/; #include <atmel/same5xx20.dtsi> #include "same54_xpro-pinctrl.dtsi" #include <zephyr/dt-bindings/input/input-event-codes.h> / { model = "SAM E54 Xplained Pro"; compatible = "same54,xpro", "atmel,same54p20a", "atmel,same54"; chosen { zephyr,console = &sercom2; zephyr,shell-uart = &sercom2; zephyr,sram = &sram0; zephyr,flash = &flash0; }; /* These aliases are provided for compatibility with samples */ aliases { led0 = &led0; pwm-led0 = &pwm_led0; sw0 = &button0; i2c-0 = &sercom7; }; leds { compatible = "gpio-leds"; led0: led_0 { gpios = <&portc 18 GPIO_ACTIVE_LOW>; label = "Yellow LED"; }; }; pwmleds { compatible = "pwm-leds"; pwm_led0: pwm_led_0 { pwms = <&tcc0 2 PWM_MSEC(20)>; }; }; buttons { compatible = "gpio-keys"; button0: button_0 { gpios = <&portb 31 (GPIO_PULL_UP | GPIO_ACTIVE_LOW)>; label = "SW0"; zephyr,code = <INPUT_KEY_0>; }; }; }; &cpu0 { clock-frequency = <120000000>; }; &tcc0 { status = "okay"; compatible = "atmel,sam0-tcc-pwm"; /* Gives a maximum period of 1.1s for 120MHz main clock */ prescaler = <8>; #pwm-cells = <2>; pinctrl-0 = <&pwm_default>; pinctrl-names = "default"; }; &rtc { status = "okay"; counter-mode = "clock"; prescaler = <1024>; atmel,assigned-clocks = <&osc32kctrl 4>; }; &sercom2 { status = "okay"; compatible = "atmel,sam0-uart"; current-speed = <115200>; rxpo = <1>; txpo = <0>; #address-cells = <1>; #size-cells = <0>; pinctrl-0 = <&sercom2_uart_default>; pinctrl-names = "default"; };&dmac { status = "okay"; };&sercom4 { status = "okay"; compatible = "atmel,sam0-spi"; dipo = <3>; dopo = <0>; #address-cells = <1>; #size-cells = <0>; pinctrl-0 = <&sercom4_spi_default>; pinctrl-names = "default";cs-gpios = <&portb 28 GPIO_ACTIVE_LOW>;/* Configure DMA */ dmas = <&dmac 0 12>, <&dmac 1 13>; dma-names = "rx", "tx";lan8651: lan8651@0 { compatible = "microchip,lan865x"; reg = <0>; int-gpios = <&portb 7 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>; rst-gpios = <&porta 6 GPIO_ACTIVE_LOW>; local-mac-address = [14 15 16 11 12 13]; spi-max-frequency = <20000000>; status = "okay"; lan865x_mdio: lan865x_mdio { compatible = "microchip,lan865x-mdio"; status = "okay"; #address-cells = <1>; #size-cells = <0>; ethernet-phy@0 { compatible = "microchip,t1s-phy"; reg = <0x0>; plca-enable; plca-node-id = <0>; plca-node-count = <8>; plca-burst-count = <0>; plca-burst-timer = <0x80>; plca-to-timer = <0x20>; status = "okay"; }; }; };}; &sercom7 { status = "okay"; compatible = "atmel,sam0-i2c"; clock-frequency = <I2C_BITRATE_FAST>; #address-cells = <1>; #size-cells = <0>; pinctrl-0 = <&sercom7_i2c_default>; pinctrl-names = "default"; eeprom: eeprom@5e { compatible = "atmel,24mac402"; reg = <0x5e>; }; }; &adc0 { status = "okay"; }; zephyr_udc0: &usb0 { status = "okay"; pinctrl-0 = <&usb_dc_default>; pinctrl-names = "default"; }; &gmac {status = "disabled";pinctrl-0 = <&gmac_rmii>; pinctrl-names = "default"; mac-eeprom = <&eeprom>; phy-handle = <&phy>; }; &mdio {status = "disabled";pinctrl-0 = <&mdio_default>; pinctrl-names = "default"; phy: ethernet-phy@0 { compatible = "ethernet-phy";status = "disabled";reg = <0>; }; }; &flash0 { partitions { compatible = "fixed-partitions"; #address-cells = <1>; #size-cells = <1>; /* * The final 16 KiB is reserved for the application. * Storage partition will be used by FCB/LittleFS/NVS * if enabled. */ storage_partition: partition@fc000 { label = "storage"; reg = <0x000fc000 0x00004000>; }; }; }; -
Save the changes.