3.5.1 Gain Table Example
The PIC32MZ2051W1 gain table is a text-based file that the user can open or edit using any text editor. The following are the rules for a gain table file:
- “
;;;” means comment entire line. - If the first character is “
;”, this row is for file information.Note: The user must not modify this row.
- If the first character is blank, it means this row has the Gain Table information. The user can modify the power target values but not other information and format.
- Gain table information power target values ranges from 10-25 dBm, each step equals 0.25 dB.
Note: If any of the information in the gain table is not available, this group of information is invalid.