32.3.3.10 Accumulator Test

The Accumulator Test mode aids in diagnostics of the accumulator and the result formatting hardware and can test the integrity of the logic. It is enabled by configuring the MODE bitfield in the Command (ADCn.COMMAND) register to ACCTEST.

The Accumulator Test mode is used as follows:
  • Writing to the Sample (ADCn.SAMPLE) register writes directly to the internal 16-bit accumulator
  • Writing to the Result (ADCn.RESULT) register accumulates the 10 LSb of the written value in the internal 16-bit accumulator
  • Reading the Result register will read the internal 16-bit accumulator
Figure 32-6. Accumulator Test
Note:
  1. If the Left Adjust (LEFTADJ) bit in the Control F (ADCn.CTRLF) register is ‘1’, a value written to the Result register will be left adjusted 6-SAMPNUM bits before accumulated.
  2. One peripheral clock (CLK_PER) clock cycle must be allowed between writing to the Result register and reading it back again. This can be achieved by executing any instruction between the write and the read operations, such as a NOP instruction.