4.4.10 Interrupt Functions
The __interrupt(type) specifier can be used to
indicate that a function is to act as an interrupt service routine. The type is a
comma-separated list of keywords that indicate information about the interrupt
function.
The current interrupt types are:
| <empty> | Implement the default interrupt function. |
|---|---|
| low_priority | The interrupt function corresponds to the low
priority interrupt source. (MPLAB XC8 - PIC18 only) |
| high_priority | The interrupt function corresponds to the high priority interrupt
source. (MPLAB XC8) |
| save(symbol-list) | Save the listed symbols on entry, and restore
on exit. (MPLAB XC16) |
| irq(irqid) | Specify the interrupt vector associated with this interrupt. (MPLAB XC16 and XC8) |
| altirq(altirqid) | Specify the alternate interrupt vector
associated with this interrupt. (MPLAB XC16) |
base(address) | Specify vector table address. (MPLAB XC8) |
| preprologue(asm) | Specify assembly code to be executed before
any compiler-generated interrupt code. (MPLAB XC16) |
| shadow | Allow the ISR to utilize the shadow registers
for context switching. (MPLAB XC16) |
| auto_psv | The ISR will set the PSVPAG register and
restore it on exit. (MPLAB XC16) |
| no_auto_psv | The ISR will not set the PSVPAG register. (MPLAB XC16) |
Use the native keywords discussed in the Differences section to look up information on the semantics of this specifier.
Some devices may not implement interrupts. Use of this qualifier
for such devices generates a warning. If the argument to the __interrupt
specifier does not make sense for the target device, a warning or error is issued by the
compiler.
Example
The following shows a function qualified using
__interrupt.
__interrupt(low_priority) void getData(void) {
if (TMR0IE && TMR0IF) {
TMR0IF=0;
++tick_count;
}
{Differences
8-bit compilers have used the interrupt and low_priority
qualifiers to indicate this meaning for some devices. Interrupt routines were, by default,
high priority. The __interrupt() specifier may now be used outside of the
CCI.
The 16-bit and 32-bit compilers have used the interrupt
attribute to define interrupt functions.
Migration to the CCI
For 8-bit compilers, change any occurrence of the interrupt qualifier,
e.g., from:
void interrupt myIsr(void)
void interrupt low_priority myLoIsr(void)to the following, respectively:
void __interrupt(high_priority) myIsr(void)
void __interrupt(low_priority) myLoIsr(void)For 16-bit compilers, change any occurrence of the
__interrupt() attribute, e.g., from:
void _attribute_((interrupt(auto_psv,irq(52))))
_T1Interrupt(void);to:
void __interrupt(auto_psv,irq(52))) _T1Interrupt(void);For 32-bit compilers, the __interrupt() keyword takes two parameters, the
vector number and the (optional) IPL value. Change code that uses the interrupt attribute,
similar to these examples:
void __attribute__((vector(0), interrupt(IPL7AUTO), nomips16))
myisr0_7A(void) {}
void __attribute__((vector(1), interrupt(IPL6SRS), nomips16))
myisr1_6SRS(void) {}
/* Determine IPL and context-saving mode at runtime */
void __attribute__((vector(2), interrupt(), nomips16))
myisr2_RUNTIME(void) {}to:
void __interrupt(0,IPL7AUTO) myisr0_7A(void) {}
void __interrupt(1,IPL6SRS) myisr1_6SRS(void) {}
/* Determine IPL and context-saving mode at runtime */
void __interrupt(2) myisr2_RUNTIME(void) {}Caveats
None.