4.4.4 Near Objects
The __near qualifier can be used to indicate that
variables or functions are located in ‘near memory’. Exactly what constitutes near memory
is dependent on the target device, but it is typically memory that can be accessed with
less complex code. Expressions involving near-qualified objects generally are faster and
result in smaller code.
Use the native keywords discussed in the Differences section to look up information on the semantics of this qualifier.
Some devices may not have such memory implemented, in which case, use of
this qualifier is ignored. Stack-based (auto and parameter) variables
cannot use the __near specifier.
Example
The following shows a variable and function qualified using
__near.
__near int serialNo;
__near int ext_getCond(int selector);
Differences
The 8-bit compilers have used the qualifier near to indicate this meaning.
Functions could not be qualified as near.
The 16-bit compilers have used the near attribute with both variables and
functions.
The 32-bit compilers have used the near attribute for functions only.
Migration to the CCI
For 8-bit compilers, change any occurrence of the near qualifier to __near,
e.g., from:
near char template[20];
to:
__near char template[20];
In 16- and 32-bit compilers, change any occurrence of the
near attribute to __near, for example, from:
void bar(void) __attribute__ ((near));
int tblIdx __attribute__ ((near));
to:
void __near bar(void);
int __near tblIdx;
Caveats
None.