4.4.5 Persistent Objects
The __persistent qualifier can be used to indicate that
variables should not be cleared by the runtime startup code.
Use the native keywords discussed in the Differences section to look up information on the semantics of this qualifier.
Example
The following shows a variable qualified using
__persistent.
__persistent int serialNo;
Differences
The 8-bit compilers have used the qualifier, persistent, to indicate this
meaning.
The 16- and 32-bit compilers have used the persistent
attribute with variables to indicate they were not to be cleared.
Migration to the CCI
With 8-bit compilers, change any occurrence of the persistent qualifier to
__persistent, e.g., from:
persistent char template[20];
to:
__persistent char template[20];
For the 16- and 32-bit compilers, change any occurrence of the persistent
attribute to __persistent, for example, from:
int tblIdx __attribute__ ((persistent));
to:
int __persistent tblIdx;
Caveats
None.