11.2.3.3 Auto Variable Size Limits
If a program requires large objects that should not be accessible to the
entire program, consider leaving them as local objects by using the
static specifier. Such variables are still local to a function, but
are no longer auto and are allocated permanent storage which is not in
the software stack.
The auto objects are subject to the similar constraints
as non-auto objects in terms of maximum size, but they are allocated to
the software stack rather than fixed memory locations. 11.2.2 Non-Auto Variable Allocation and Access, Non-Auto Variable
Size Limits. which describes defining and using large arrays is also applicable to
auto objects.