11.3.1.1 String and Const Objects
By default, the compiler will automatically arrange for strings and
const-qualified initialized variables to be allocated in the
auto_psv section, which is mapped into the PSV window. Specify the
-mconst-in-data option to direct the compiler not to use the PSV
window and these objects will be allocated along with other RAM-based variables.
In the default memory model, the PSV page is fixed to one page which is
represented by the auto_psv memory space. Accessing the single auto PSV
page is efficient as no page manipulation is required. Additional Flash may be accessed
using the techniques introduced in section 11.3.2 Access of Objects in Program Memory, Managed PSV
Access.