11.4.1 Initialize PMP
The PMP peripheral requires initialization before any access can be properly processed. Consult the appropriate documentation for the device you are interfacing to and the data sheet for DSC device you are using.
If PMP is used, the toolsuite will call void
__init_PMP(void) during normal C run-time initialization. If a customized
initialization is being used, please ensure that this function is called.
This function should make the necessary settings in the PMMODE and PMCON SFRs. In particular:
- The peripheral should not be configured to generate interrupts:
PMMODEbits.IRQM = 0 - The peripheral should not be configured to generate increments:
PMMODEbits.INCM = 0The compiler will modify this setting during run-time as needed. - The peripheral should be initialized to 16-bit mode:
PMMODEbits.MODE16 = 1The compiler will modify this setting during run-time as needed. - The peripheral should be configured for one of the MASTER modes:
PMMODEbits.MODE = 2orPMMODEbits.MODE = 3 - Set the wait-states
PMMODEbits.WAITB,PMMODEbits.WAITM, andPMMODEbits.WAITEas appropriate for the device being connected. - The PMCON SFR should be configured as appropriate making sure that
the chip select function bits
PMCONbits.CSFmatch the information communicated to the compiler when defining memory spaces.
A partial example might be:
void __init_PMP(void) {
PMMODEbits.IRQM = 0;
PMMODEbits.INCM = 0;
PMMODEbits.MODE16 = 1;
PMMODEbits.MODE = 3;
/* device specific configuration of PMMODE and PMCCON follows */
}