25.3.13 Default Bit-field int
Type
The type of a bit-field specified as a plain int is identical to that of
one defined using unsigned int. This is quite different from other
objects where the types int, signed and signed
int are synonymous. It is recommended that the signedness of the bit-field
be explicitly stated in all bit-field definitions.
Example
The following shows an example of a structure tag containing bit-fields that are unsigned integers and with the size specified.
struct OUTPUTS {
int direction :1;
int parity :3;
int value :4;
};
Differences
When targeting PIC devices, the MPLAB XC8 compiler has issued a warning if an
int type was specified for bit-fields, and it has instead
implemented the bit-field with an unsigned int type. For other devices,
this compiler has implemented bit-fields defined using int as having a
signed int type, unless the option
-funsigned-bitfields was specified. Use of a signed
int type is also true for the MPLAB XC16, XC-DSC, and XC32 compilers.
Migration to the CCI
Any code that defines a bit-field with the plain int type should be
reviewed. If the intention was for these to be signed quantities, then the type of these
should be changed to signed int. In the following example:
struct WAYPT {
int log :3;
int direction :4;
};
the bit-field type should be changed to signed int, as in:
struct WAYPT {
signed int log :3;
signed int direction :4;
};