1.2 Conventions Used in This Guide
The following conventions may appear in this documentation. In most cases, formatting conforms to the OASIS Darwin Information Typing Architecture (DITA) Version 1.3 Part 3: All-Inclusive Edition, 19 June 2018.
| Description | Implementation | Examples |
|---|---|---|
| References | DITA: cite | MPLAB® XC-DSC C/C++ Compiler User’s Guide for dsPIC33C/E/F and dsPIC30 DSC. |
| Emphasized text | Italics | ...is the only compiler... |
| A window, window pane or dialog name. | DITA: wintitle | the
Output window. the New Watch dialog. |
| A field name in a window or dialog. | DITA: uicontrol | Select the Optimizations option category. |
| A menu name or item. | DITA: uicontrol | Select the File menu and then Save. |
| A menu path. | DITA: menucascade, uicontrol | |
| A tab | DITA: uicontrol | Click the Power tab. |
| A software button. | DITA: uicontrol | Click the OK button. |
| A key on the keyboard. | DITA: uicontrol | Press the F1 key. |
| File names and paths. | DITA: filepath | C:/Users/User1/Projects |
| Source code: inline. | DITA: codeph | Remember to
#define START at the beginning of your
code. |
| Source code: block. | DITA: codeblock | An example
is: |
| User-entered data. | DITA: userinput | Type in a device name, for example PIC18F47Q10. |
| Keywords | DITA: codeph | static, auto,
extern |
| Command-line options. | DITA: codeph | -Opa+, -Opa- |
| Bit values | DITA: codeph | 0,
1 |
| Constants | DITA: codeph | 0xFF,
'A' |
| A variable argument. | DITA: codeph + option | file.o, where
file can be any valid file
name. |
| Optional arguments | Square brackets [ ] | xc8
[options]
files |
| Choice of mutually exclusive arguments; an OR selection. | Curly brackets and pipe character: { | } | errorlevel {0|1} |
| Replaces repeated text. | Ellipses... | var_name [,
var_name...] |
| Represents code supplied by user. | Ellipses... | void
main (void)
|
| A number in verilog format, where N is the total number of digits, R is the radix and n is a digit. | N‘Rnnnn | 4‘b0010, 2‘hF1 |
| Device Dependent insignia. Specifies that a feature is not supported on all devices. Please see your device data sheet for details. | [DD] | Assembler Special Operators |