11.3.2 Automatically Allocating Objects into Program Space
When the option -mconst-in-code is enabled,
const-qualified variables that are not auto are
placed in program memory. Any auto variables qualified
const are placed on the stack along with other
auto variables.
Any const-qualified (auto or
non-auto) variable will always be read-only and any attempt to
write to these in your source code will result in an error being issued by the
compiler.
A const object is usually defined with initial values,
as the program cannot write to these objects at runtime. However this is not a
requirement. An uninitialized const object is allocated space along
with other uninitialized RAM variables, but is still read-only. Here are examples of
const object definitions.
const char IOtype = ’A’; // initialized const
object
const char buffer[10]; // I reserve memory in RAM
See the 17 Mixing C/C++ and Assembly Code section for the equivalent assembly symbols that are used to
represent const-qualified variables in program memory.