1.1.2.3.1.1.4.7 BLE_ANCS_PerformNtfyAction
C
uint16_t BLE_ANCS_PerformNtfyAction(uint16_t connHandle, uint32_t ntfyId, BLE_ANCS_ActionId_T actId);Description
Function for The Perform Notification Action command allows an NC to perform a predetermined action on a specific iOS notification.
Parameters
| Parameter | Description |
|---|---|
| [in] connHandle | The connection handle. |
| [in] ntfyId | A 32-bit numerical value representing the UID of the iOS notification on which the client wants to perform an action. The ntfyId could be retrieved when receiving BLE_ANCS_EVT_NTFY_ADDED_IND or BLE_ANCS_EVT_NTFY_MODIFIED_IND or BLE_ANCS_EVT_NTFY_REMOVED_IND events. |
| [in] actId | The desired action the NC wants to be performed on the iOS notification. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully complete the API. |
| MBA_RES_FAIL | Operation is not permitted. |
| MBA_RES_OOM | No available buffer. |
| MBA_RES_INVALID_PARA | Invalid parameters. One of the following reasons: - Connection handle is not valid - Invalid write parameters. See GATTC_WriteParams_T for valid values. |
| MBA_RES_NO_RESOURCE | No available resource to send write operation. |
| MBA_RES_BUSY | GATT Client is busy. Another request is ongoing. |