1.2.2.1.3.4.6 BLE_L2CAP_CbPauseAuthorization
C
uint16_t BLE_L2CAP_CbPauseAuthorization(uint16_t spsm, bool enable);Description
Pause or resume authorization in specific SPSM.
Note
All SPSMs are all authorized as default. Use this API to pause the authorization if required.
Parameters
| Parameter | Description |
|---|---|
| [in] spsm | Simplified Protocol/Service Multiplexer. |
| [in] enable | Set true to pause the authorization (unauthorized). Otherwise, authorized. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully configure the SPSM. |
| MBA_RES_INVALID_PARA | Unknown SPSM. |