BLE_TRSPS_SendVendorCommand
C
uint16_t BLE_TRSPS_SendVendorCommand(uint16_t connHandle, uint8_t commandID, uint8_t commandLength, uint8_t *p_commandPayload);
Description
Send vendor command.
Parameters
Parameter | Description |
---|---|
[in] connHandle | Connection handle associated with this connection. |
[in] commandID | Command id of the vendor command. |
[in] commandLength | Length of payload in vendor commnad. |
[in] p_commandPayload | Pointer to the payload of vendor command. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | Successfully issue a send vendor command. |
MBA_RES_FAIL | Invalid connection. |
MBA_RES_OOM | No available memory. |
MBA_RES_INVALID_PARA | Error commandID usage or commandLength invalid or the CCCD of TCP is not enabled. |