BLE_DTM_TransmitterTestParams_T
C
typedef struct BLE_DTM_TransmitterTestParams_T { uint8_t txChannel; uint8_t testDataLen; uint8_t packetPayload; uint8_t phy; int8_t transmitPowerLevel; } BLE_DTM_TransmitterTestParams_T;
Description
Transmitter test parameters.
Field Documentation
Field | Description |
---|---|
txChannel | The RF channel which is used by the transmitter. Channel= (F – 2402) / 2 (Frequency Range : 2402 MHz to 2480 MHz) See Receiver or transmitter channel. |
testDataLen | The length of the Payload of the test reference packets. |
packetPayload | The contents of the Payload of the test reference packets. See Transmitter payload type. |
phy | The PHY which is used by the transmitter. See Transmitter PHY type. |
transmitPowerLevel | The transmit power level which is used by the transmitter. Range: -127 to +20. (Units: dBm) Set to 0x7E to use the minimum transmit power level. Set to 0x7F to use the maximum transmit power level. If the parameter is set to a value other than 0x7E or 0x7F, then ble stack makes the requested change or makes closest change that it is capable of doing. |