BLE_DM_PairedDevInfo_T
C
typedef struct BLE_DM_PairedDevInfo_T
{
BLE_GAP_Addr_T remoteAddr;
uint8_t remoteIrk[16];
BLE_GAP_Addr_T localAddr;
uint8_t localIrk[16];
uint8_t rv[8];
uint8_t ediv[2];
uint8_t ltk[16];
unsigned int lesc:1;
unsigned int auth:1;
unsigned int encryptKeySize:6;
}BLE_DM_PairedDevInfo_T;Description
Structure for containing information about paired device information.
Field Documentation
| Field | Description |
|---|---|
| remoteAddr | Bluetooth address of the paired device. See BLE_GAP_Addr_T for structure details. |
| remoteIrk | Identity resolving key of the paired device. |
| localAddr | Bluetooth address of the local device. See BLE_GAP_Addr_T for structure details. |
| localIrk | Identity resolving key of the local device. |
| rv | Random value used in the pairing process. |
| ediv | Encrypted diversifier used in the pairing process. |
| ltk | Long term key for the BLE link. |
| lesc | Indicates use of LE secure connection if set. |
| auth | Indicates authenticated pairing if set. |
| encryptKeySize | Encryption key size (7-16 bytes). |