BLE_OTAPC_DeviceReset
C
uint16_t BLE_OTAPC_DeviceReset(uint16_t connHandle);Description
Requests a device reset on the server device after OTA DFU.
Parameters
| Parameter | Description |
|---|---|
| [in] connHandle | Handle of the connection for device reset request. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Device reset request initiated successfully. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_INVALID_PARA | The provided connection handle is not valid. |
| MBA_RES_BAD_STATE | The OTA profile is not in the correct state to perform this operation. |