BLE_OTAPC_UpdateRequest
C
uint16_t BLE_OTAPC_UpdateRequest(uint16_t connHandle, BLE_OTAPC_Req_T * p_req);Description
Initiates a firmware update request operation.
Note
An event of type BLE_OTAPC_EVT_REQ_RSP_IND will be generated upon completion of the procedure.
Parameters
| Parameter | Description |
|---|---|
| [in] connHandle | The connection handle for which to perform the firmware update request operation. |
| [in] p_req | Pointer to the request parameters to send to the server. See BLE_OTAPC_Req_T. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | The start of the firmware update request operation was successful. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_INVALID_PARA | The provided connection handle is not valid. |
| MBA_RES_BAD_STATE | The OTA profile is not in the correct state to perform this operation. |