BLE_OTAPC_EventCb_T
C
typedef void(*BLE_OTAPC_EventCb_T)(BLE_OTAPC_Event_T *p_event);
Description
Callback type for BLE OTA (Over-The-Air) profile events.
Note
This callback function is used to forward BLE OTA profile events to the application layer. When an event occurs, this function will be invoked with a pointer to the event data structure.
Parameters
| Parameter | Description |
|---|---|
| [in] p_event | Pointer to the BLE_OTAPC_Event_T structure containing event details. |