3.2 B6.ER2 LOCK(0x8A) Error After an Interrupted Delete Command

Issue Description

A Create after an interrupted Delete may result in locked handles. Deleting or writing to a handle may return a Lock error.

Work Around

To avoid this issue, the device must NOT be reset during execution of critical commands such as Create and Delete. These commands must be allowed to run to completion. Execution time depends on the size of the handle being created or deleted.

Corrective Actions

This issue has been resolved in Patch P5.