4.2 Theory of Operation
The DAC is used to create a current source. Although the DAC outputs a voltage signal V0, the resistors in the circuit will create a current I0 that is given by:
The voltage divider rule gives the following equation for the voltage drop across RSENSE:
If the expression for I0 is substituted (the same current flows through all the resistors), the following expression is obtained:
This, in turn, leads to:
Since RSENSE is known, measuring the voltage drop across RSENSE may determine the current.
With the output voltage V0 set to 1V (DAC0 OUT) and using the resistor values as listed, the following result is obtained: