When the key “a” is entered, the
terminal window will appear as shown in the following figure
Then, the device will disable the
tamper operation and enable the RTC
After enabling the RTC, the firmware
will turn off the LCD backlight (turns on LED) and wait for the next input from the
user
Providing tamper by pressing SW0
shall not be detected by the device
Figure 6-5. Terminal Window when Tamper
Disabled
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.