When the key “b” is entered, the
terminal window will appear as shown in the following figure
Figure 6-6. Terminal Window when
Tamper Enabled in Wake Mode
The device will enable the tamper
detection in wake mode (for more details, refer Modes of Operation ) and enable the RTC
After enabling the RTC, the clock
starts counting at an interval of 1 second
Set the mode flag and the previous
mode flag as SET_TO_WAKE, to keep track of the current operating
mode of tamper and previous mode of tamper
The device goes to sleep. However,
the RTC will still be running internally.
Here, the Tamper condition can be
generated by press and release of the user switch SW0 (which is connected to the
tamper input pin)
When a tamper is detected, the device
wakes from sleep mode. The firmware will stay awake to detect future tamper inputs.
The user also has the provision to change the input mode only after the first tamper
condition is detected.
Once the tamper occurs, the following
action happens:
Displays the error message
“Tamper occurred” to indicate that tamper has occurred as shown in the
following figure
Figure 6-7. Terminal
Window when Tamper Callback Occured in Wake Mode
The device remains awake,
detects tampers or key pressed by the user, and performs the actions
accordingly
It turns OFF LED and turns ON
LCD backlight
Get the current time from the
clock register and sets alarm after five seconds
Set the tamper flag
Display the error message
“TAMPR” on the LCD as shown in the following figure and enable the timer
module with specified overflow value (user configurable) for blinking the
SLCD backlight by toggling the port pin connected to it
Figure 6-8. LCD Screen
when Tamper Occured in Wake Mode
Comes to alarm call back
after five seconds where the firmware clears the LCD display and disables
the TCC (timer module to stop LCD backlight blinking). Now, the device is
ready for next the tamper condition or other operations.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.