3.10.4 SleepWalking Application on SAM E54 Xplained Pro Evaluation Kit
Description
This application demonstrates SleepWalking using the Event System. The application uses an ADC with a Window Monitoring feature in Standby mode for the following use cases:
- Standby mode with Interrupts (IRQ)
- Standby mode with Event System
(SleepWalking)
On power up, the application is in STDBY_IRQ_MODE. It is possible to switch from STDBY_IRQ_MODE to STDBY_EVSYS_MODE by pressing the switch button (SW0) embedded on the SAM E54 Xplained Pro board. The application wakes up from Sleep mode and enters into ACTIVE_MODE when the embedded light sensor on the I/O1 Xplained Pro extension kit is covered.
Modules/Technology Used
- Peripheral Modules:
- ADC
- CMCC
- DMAC
- EVSYS
- NVMCTRL
- PM
- RTC
- SERCOM
- SUPC
- SYSTICK
- STDIO Library
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer Project Manifest present in harmony-manifest-success.yml under the project folder firmware/src/config/sam_e54_xpro.
- Refer the Release Notes to know the MPLAB X IDE and MCC Plugin version.
- Any Serial Terminal application, such as Tera Term terminal application.
- MPLAB Data Visualizer .
Because Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Ensure jumper to measure MCU current is set to MEASURE.
- Ensure jumper to measure I/O current is set to BYPASS.
- Connect the I/O1 Xplained Pro Extension Kit to the EXT XPRO connector 2 on the SAM E54 Xplained Pro Evaluation Kit.
- Connect the micro USB cable from the
computer to the DEBUG USB connector on the SAM E54 Xplained Pro Evaluation Kit.
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened.
- Go to File -> Import -> Hex/ELF File.
- In the Import Image File
window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file.
- Select Device as ATSAME54P20A.
- Ensure the proper tool is selected under Hardware Tool and click on Next button.
- Select Project Name and Folder,
- Select appropriate project name and folder and click on Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click on Make and Program Device button to program the device.
- Follow the steps in Running the Demo section below.
Programming/Debugging Application Project
- Open the project (sleepwalking\firmware\sam_e54_xpro.X) in MPLAB X IDE
- Ensure SAM E54 Xplained Pro is selected as hardware tool to program/debug the application
- Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo
- Open Tera Term or any equivalent serial communication tool.
- In the Tera Term: New Connection window, select the Serial Port number allocated to the connected SAM E54.
- Configure the Tera Term Serial port interface to 115200 speed.
- Reset the board by pressing the reset
button. The application will start by displaying the following message on the serial
terminal.

- Open the MPLAB Data Visualizer (from MPLAB X IDE) and SAM E54 Xplained Pro is visible on the Connections Control Panel
- In the MPLAB Data Visualizer tab, different interfaces will appear under the SAM E54
Xplained Pro.
- Select the Power interface and click on the Power Settings button. Then, click on
Calibrate.

- Once calibration is completed, click
on the Start Capturing Power button. A window will pop up; select Plot Raw and then
click Close.

- The MPLAB Data Visualizer will display the power consumption details in the Power
Analysis window.
- When the application starts, the device will run on Standby with IRQ mode. The data analyzer shows the power consumption of the device when the CPU is woken up every 10 milliseconds by an RTC Compare ‘0’ interrupt to start an ADC conversion.
- Using the SW0 push button, it is possible to change the application mode from Standby with IRQ to SleepWalking. In this mode the CPU is woken up only when an ADC window monitoring interrupt occurs. The data analyzer shows the power consumption of the device when running in Standby with the Event System (SleepWalking).
Comments
- Reference Application Note: SleepWalking with Event System Using the SAM E54 (DS00003342).
- Getting Started Training Module: Getting Started with Harmony v3 Peripheral Libraries on SAM D5x/E5x MCUs
- This application demo builds and
works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo, should use the
MPLAB Harmony v3 Software framework. Refer links below to setup and build the
applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232).
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253).
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project